Part Number: BQ24010
Hello,
We want to charge a 1-cell Li-Po Battery with 250mA charging current through a USB 2.0 input. Issue is that as the battery charges the charging current reduces.
With C4 (Capacitor at Vcc pin)= 100nF
Batt=3.5 Charging current=161mA
Batt=3.304 Charging current=176mA
Batt=3.165 Charging current=223mA
With C4 (Cap at Vcc pin)=10uF
Batt=4V Charging current=138mA
Batt=3.402 Charging current=223mA
Batt=3.256 Charging current=250mA
Batt=3.068 Charging current=253mA
What can be the reason that charging current doesnt stay constant?
Please find the schematic below: