Other Parts Discussed in Thread: BQ29312A
dear teacher
pls give the idea...
we use the BQ2084-V143 solution. (BQ2084 + BQ29312APW ; http://www.ti.com/lit/ds/symlink/bq2084-v143.pdf )
our question is regarding " BQ29312APW " 's operation with abnormal.
==> Question
using condition : series array 4 battery pack
==> problem
3'st or 4'st battery measured voltage is 1.5V or 7V
make separated the battery then each one'w battery's measure voltage values is 4.2V.
Q1. what's is problem?
Q2. BQ29312APW's fault operation can check without battery connection?