Greetings,
We managed to form a DC to DC Convertor circuit using PTH08T231W.
Please check the attached data.
Structures are like below :
input voltage : 12V Linear DC Power Supply (E3632A Agilent)
output : 5V/5A
Question 1.
Input current is 70mA without a load.
we cannot obtain specifications of output ON condition in Data sheet.
Please check whether this is activating properly.
Question 2.
When there is a load with 5V/5A, ripple is much higher than we expected.
We'd like to have at least 50mV p-p, is this possible?
If it is possible, can external components can be involved?
and how can we make at least 50mV p-p?