This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069 For Current Limit

Other Parts Discussed in Thread: LM5069

I'm looking at an application that needs to pass 8A during normal operation yet trip at 8.5A.  The LM5069 would seem close but the tolerance of the current limit threshold voltage is 48.5 to 61.5mV.  In order to make sure 8A is always passed I'd have to design to roughly (.0485/8) = .006 ohms.  The max the part could then trip at is (.0615 / .006) = 10.25A.

Are there any other parts that pull the tolerance in or are the design requirements unrealistic?