Part Number: LM5576
Hi team,
[Q1]
Could you tell me the definition of Boost UVLO. Is following correct?
- Boost UVLO: UVLO is activated when the BST-SW pin voltage falls below voltage of Boost UVLO.
- BOOST UVLO Hysteresis: The hysteresis voltage is the voltage difference between when the UVLO is activated and when it is deactivated.
So, assuming typical values, UVLO is activated when the BST-SW pin voltage falls below 3.8V, and the UVLO is deactivated when the voltage exceeds 4.6V (3.8V + 0.8V), correct?
[Q2]
What is the maximum value of Boost UVLO?

Best regards,
Goto