I have a 4 phase pfc and I am having a problem. One of the channels from the same IC has a different duty ratio then the other so it is not sharing current (the current is discontinuous in that phase). All other 3 phase have continuous current. It is not that the inductors are different since the on time of that particular channel is much less than the other 3. In other words, the on time of GDA is different then GDB. So much so that the current is discontinuous
Any ideas why this may happen? All the component seem correct and there is no sign of instability
Please advise