I have a BQ77910 chip and having difficulty communicating with it. I purchased the chip, not the EVM. I got a breakout board made so I can test it on a breadboard, and I have already checked that there are no shorts or opens. I also purchased the USB-GPIO Module and updated it accordingly. I'm using a 64-bit Win 7 machine.
My difficulty is what to do next. I have not found an explicit set of insturctions to plug in and communicate with the chip directly. Generally, I have all the GND, VSS, and GPIO GND all tied together, BAT and CHGSTS about 12V, DATA and CLK tied directly to the GPIO lines, and ZEDE tied directly to the GPIO line.
The version of the software I have is defaulted to communicate with BQ77908, and it always says Cannot Find Target BQ77908. But, the software won't let me select the BQ77910 option.
Also, I've noticed a 'Comm Status: Driver Error' at the bottom status line when its searching for the target.
Outside of recheck your wires, does anyone have some suggestions or recommendations?