Part Number: TPSM828301
Other Parts Discussed in Thread: TPSM828302,
Page 12 of April2025 datasheet says:
"Larger output voltage combined with large output capacitance can trigger an over current event and prevent the device from starting up correctly. The circuit designer needs to select the maximum output capacitance in accordance to the target output voltage and start-up time."
Your WEBENCH design for my application suggests 22uF output capacitance - but my SoC/ASIC circuits could add another 150uF.
1) How to determine maximum output capacitance that allows device to start up correctly?
2) Will using TPSM828302 instead of TPSM828301 help prevent startup problems due to high output capacitance?