Part Number: UCC28780
I'm working on a new design with the UCC28780. Startup is going through the normal sequence until it gets to the step where the RUN pin is supposed to go high. Run doesn't go high and PWML never goes high. VDD continues to drop until it gets low enough (about 8ms), and then it recharges with the SWS pin, and this cycle continues. I checked the Chvg is 2.2nF and it's fall time to 11V is much greater than 25us. Vref is going to 5V. And I couldn't find evidence that any of the other shutdowns were causing this. Do you have any suggestions for troubleshooting this?