Part Number: TLV774
Hello,
In a circuit design using the TLV77433, due to system limitations, a voltage of 0.9V sneaks into VOUT from an external source during the approximately 900ms period when VIN is 0V after power-on. The reverse current value at this time is limited to less than 0.4mA. According to the datasheet, to avoid damaging the device, the reverse current should be limited to less than 5% of the rated current for a short period of time. I believe 0.4mA meets this condition, but does 900ms fall within the short-term range? I am considering an application where the power supply will be started up several times a day.
Kind regards,
Yas