This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV7308: can support external driver?

Part Number: DRV7308

Hi Team,

 

According to the SPEC, the 6-channel PWM control signals of the DRV7308 can accept 15V level input control.

Please help confirm whether the DRV7308 can also be individually controlled using PWM outputs from a driver IC with a predriver?

This is a redundancy design question, please help to check, thank you!