hi,
I am Umesh, I have question regarding PMIC (TPS65950) power consumtion during backup mode. We are using HB414IV01E (Seiko instruments) backup battery, Which is having Nominal capacity of 150 uAh capacity @ 5 uA if operating voltage is 3 to 2 V .
From the datasheet of TPS65950A3 (Table 4.4 in Data Manual) , we can notice that current consumption in backup mode is 2.25uA, Which can be provided by HB414IV01E backup battery .But we are loosing backup battery capacity very quickly not even 6 hours. According to data we have, backup battery must work around 65 hours.
I have question "Is PMIC drawing more current in backup mode?"
or
"Is there any other factor of PMIC which decides the Battery performance"
Can you clear this doubt ...
Thank you
Umesh