This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to get maximum efficiency in TPS65251.

Other Parts Discussed in Thread: TPS65251, TPS65253

Hi ,

One of our customer is developing a hand held POS based on TPS65251 PMIC and rail are follows ........ customer is not getting the efficiency in Light load  . how we have to increase the efficiency in each BUCK ?  Do we have any better PMIC with better efficiency ?

9 V to 12 V / 3 A (Lithium ion battery ) ------------------------------------ 5 V / 0.200 ma (BUCK 1 )& 3.3 V / 0.200 ma (BUCK 2  ) & 4.2 V / 2 A maximum (BUCK 3 ) . They want to have more efficiency in BUCK 1 & BUCK 2. 

Please suggest the solution or better device ASAP.

Regards/

Vengat.