This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

500W 650VA LLC HALF BRIDGE STEP-UP DC-DC CONVERTER using UCC25600

Other Parts Discussed in Thread: UCC25600

Pl, refer to my design and assist me further for prototyping hi-efficiency 500W 650VA LLC HALF BRIDGE STEP-UP DC-DC CONVERTER with fsw 60kHz.

Design param

Vin_min: 10,5V

Vo_max: 375V

Io-max: 1,35A

  1. Can I use MOSFET for primary side with zener anti-parallel diode (body diode)?
  2. I will be using EER3542 ferrite core transformer, so what do you suggest about Lm and Lr?
  3. Do you consider 1:50:50 turns ratio suitable?
Pl, assist me to complete my design.