This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: Update status 0x4

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQSTUDIO

Hi Team,

Posting on behalf of our customer.

I am working with a 3s3p battery pack built using Molicell INR18650-M35A cells. I recorded a log at a pack voltage of 12.6 V (4.2 V per cell), and based on that data I was recommended ChemID 7607 with a 97% match.

I am running the learning cycle: I enable the gauge, perform a full discharge, and then let the pack relax for 5 hours. However, the Update Status does not change to 0x05.

I have a question regarding my system conditions. In my application, the battery pack is charged only up to 12.45 V (4.15 V per cell), with a taper current of 350 mA. When I run the learning cycle at this voltage, Qmax does update, but the Update Status still does not transition to 0x05, even after waiting up to 5 hours.

Am I performing the procedure correctly? Or should I first complete the learning cycle at 12.6 V and then reduce the charge voltage afterward? Alternatively, should I be selecting or generating a ChemID specifically for operation at 4.15 V per cell?

Regards,

Danilo

  • Hello,

    This question has been assigned within the team and will be reviewed and followed up with another application engineer when possible. In the meantime please attach any associated .log/.gg files associated with the projects

    Thank you,
    Alan 

  • Hello Danilo,

    Based on my understanding of your post: You are stuck at the 1st discharge of the learning cycle.

    Can you please provide a datalog of your learning cycle? That way I can get a more accurate response on what might be happening.

    Am I performing the procedure correctly? Or should I first complete the learning cycle at 12.6 V and then reduce the charge voltage afterward?
    • When your battery is empty make sure:
      • Make sure the voltage of the cell does recover once the load is released.
      • The FD bit is triggered
      • The SoC reported is 0
      • Dod0 updates as a OCV measurement is taken. This is a column in the datalog from BQstudio.
      • You might need to wait longer than 5hrs depending on your battery chemistry.
    should I be selecting or generating a ChemID specifically for operation at 4.15 V per cell?

    No. if your ChemID is within 3% Dod error, then you should be fine.

    Or should I first complete the learning cycle at 12.6 V and then reduce the charge voltage afterward?

    No. your learning cycle should work fine at any charging voltage as long it is matching the ChemID.