This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM65625-Q1: Input Capacitor Selection In 48V System

Part Number: LM65625-Q1

Hi team,

I'd like to how to select input capacitor in 48V system application. In datasheet, there is only a example of 24V input.

VIN: 36~64V

VOU: 5V

IOUT: 50mA

Ripple rate: 30%

FSW: 2.2MHz

 

Regards,

Eileen