Part Number: LM25148
Hello.
I have a problem with my power supply design. When connected to a load, the power supply continues to operate at a frequency of 25 kHz. According to the RT resistor setting, we expected a frequency of 270 kHz. Without a load, I consider this OK since the PFM mode changes the frequency. However, even with a 10 A load, the frequency remains so low, the output voltage is then rippled, and at the SW node I measure large spikes before the PWM pulse. Thank for you help.
this is mi schematic

This is my osciloscope diagram, Green line is SW , Yellow is a output current, Blue is a output Voltage