Part Number: LM5148
Other Parts Discussed in Thread: TEST2,
Hello Specialist,
[Issue]
In my testing, the system enters OCP earlier than expected.
[Test condition]
Vin=24V, 30V & 36V (VDD_SRC)
Vout=12V (Measure by VOM)
Switching frequency=678kHz
Rsense=5m ohm
Choke=4.7uH ( DCR=7m ohm, Irms=13.5A, Isat=26A)
Test1:
Vin = 24V, Vout = 12V
- Load current from 1A to 7.5A: output is 12V
- At 8A load: output voltage drops to ~7V
Test2:
Vin = 30V, Vout = 12V
- Load current from 1A to 6A: output is 12V
- At 7A load: output voltage drops to ~10V
Test3:
Vin = 36V, Vout = 12V
- Load current from 1A to 6A: output is 12V
- At 7A load: output voltage drops to ~10V
Test4:
Modify C158 to 820pF, the results remain the same as in the previous tests.
Test5:
Modify Fsw 350kHz , the results remain the same as in the previous tests.
Any recommend what to check or improve to avoid early OCP triggering?