I have a BQ2004H chip and it seems to not be exiting the Hold-off period after entering fast charge mode.
Upon startup, the following steps happen:
1) LED1 stays low and LED2 pulses 1/8s high, 1/8s low for a few seconds.
2) LED1 stays low and LED2 goes high.
3) Pulse train on MOD pin of 12% duty cycle with 260uS high.
Table 1 indicates the hold of period should be 273 seconds but I have let the chip run for about 30 minutes and MOD is still behaving as seen in step 3 above. Does anyone know why this seems to be stuck in the hold-off period? How is the safety time used? Does this stop fast-charge after 650 minutes?
With relevant values:
TM1, TM2 = Vss
temp:
TS = 1.92V
VLTF = 2v
VHTF =1.46V
VTCO = 1.19V
batt voltages:
Vmcv = 4v
Vedv = 2v
Vbat = 2.475v
Vsns = Vss