Part Number: BQ25690
Hi Tema,
our customer is planning to use the BQ25690 for a superCap application, and we have the following question:
1. 6S1P 100F, voltage ration rating 2.3V, so total voltage rating is 13.8V
2. System working voltage, 13.8~8V
3. Input 5V/900mA, or 12V(nice to have)
So we need to put VREG to be very close to 13.8V, no less than 13.4V. Is it possible to using HW setting only for BQ25690? Or need FW setting, how without let cap to be over voltage?