This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51610: LMR51610XDBVR application

Part Number: LMR51610

Dear Sir/Madam,

I have a question about my application when using LMR51610XDBVR
In my circuit, there is a 24Vac (18-30Vac) which is rectified by a full bridge diode to become a DC voltage with ripple to supply to LMR51610XDBVR to regulate 5Vdc
my Unregulated DC (the input voltage of LMR51610 will vary from min.8.86V - max.41V  with 120Hz, may I know if LMR51610XDBVR can still regulate at 5V? any impact to the output voltage ripple ?

Thanks and Regards,

Kelvin