Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO

Hi,
I am trying to run learning cycle on bq34z100-g1 EVM for my battery(3S, 5000mAh), but facing some issues.
- I have run voltage calibration many times on my evm but this time it shows error(failed to enter calibration mode with command 0x2D) . SS is attached. I tried enter calibration command.
2. What is relation between voltage divider resistors and voltage divider value in bq studio?
And what should be the input voltage at pin 4 (BAT)?
3. After calibration, some parameters like cc gain, cc offset, voltage divider gets changed. how can i verify if that are correct?
4. what is difference between files with .rom, .srec and .gg extensions?
5. In which case, should i use IT_ENABLE(impedence track algorithm)?
Please help me get started.
Thank You