Hello,
I am going to use an LM5015 in the 1:1 isolated configuration (data sheet, page 21), as I need a 12V isolated output from a 12V non-isolated input.
The schematics at page 21 matches almost exactly my application needs (12 V isolated output, 200 mA maximum current), so I suppose I can use all the parts and values in that schematics.
The problem is I cannot find CHSHS-3 and CMSHS-3 diodes (... typo?), and I don't know how to dimension the 1:2 transformer and 100 uH inductor which are used.
Can someone help?
Thanks in advance,
Stefano