Part Number: LM5171-Q1
Other Parts Discussed in Thread: LM5171, LM5171EVM-BIDIR
Hello
I have a question regarding bidirectional operation under transient conditions, especially when handling inductive load turn-off.
In my system, both a resistive load and an inductive load are connected to VOUT.
When the inductive load is turned OFF, a back-EMF is generated, which causes:
- a temporary increase in VOUT (above nominal 14V)
- and a reversal of inductor current
To handle this, I am considering two methods:
1) Dynamically changing the DIR pin from HIGH (>2V, buck mode) to LOW (<1V, boost mode)
2) Keeping DIR fixed (buck mode) and allowing current direction to change by controlling ISET
My questions are:
1) Is it recommended to toggle DIR during such transient events, considering the internal soft-start/reset behavior?
2) Alternatively, is it better to keep DIR fixed and rely on ISET to handle current reversal during bidirectional operation?
3) In the ISET-based approach, can the device naturally absorb reverse current (from inductive kickback) without explicitly switching DIR?
Additionally, during this event, the resistive load remains connected to VOUT.
Should I be concerned about output voltage interruption or instability affecting the resistive load?
I would appreciate your guidance on the preferred control strategy for this situation.
Best regards,