Customer will use adaptor or USB for charger IC input, but they will never be connected to in port of bq24160, all input (USB or adaptor) need be connected USB port of bq24160.
so customer need know what is connected to USB port of bq24160.
Question is : they must set at DEFAULT mode when they use APSD(automatic power source detection).
Then anytime they read the register of memory location 3 (B4-B6). It should be 000.
So they don’t know the input power type. The charge from SPD is still very slow.
and they give me a example of other IC, i will send you the mail, maybe you could easy to know the customer requirement.
thanks!