Dear Power Community,
I would like to apply the LM5518Q in a boost configuration, converting 5V to 5.5V at max. output current of 2A. The input will be driven by a not very stable power supply, specified to be 5V +/- 0.5V. In the worst case condition the LM5118 would have to start up with 4.5V. Now I see in the datasheet, that the LM5118 cicuitry can be designed to operate with VIN less than 4 Volts, but VIN must be at least 5.00V during startup. The data sheet describes a "workaround" by increasing the input capacitance to at least 100uF, but still requiring >5.00V for startup. However doing this will increase the inrush current to values, which I can not accomodate. I tried the design and it will start up at 4,85V with input capacitance of 33uF, but how reliable is this situation? Is the startup behaviour temperature dependent?
Using the WEBENCH I can design a power supply with my desired input conditions and it does not give me any warning about input voltage violation.
Would it be advisable to use an LM3478 or LM3481 for my problem? They are however not available in automotive grade, which would be highly desirable for my application.
Thank you very much in advance for any comment.
Kind regards, Ralph.