Part Number: TPS1663

-
Disabled slow ramp up: Removed C312
-
Added a startup delay: Changed R320 to 132kR, added another 132kR in series to COM. Added a 2.2uF cap from nSHDN to COM.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS1663


Hi,
It seems like a thermal shutdown.
few follow up questions:
1) without downstream load is the device powering up properly? if you haven't tested yet, can you test without downstream load?
2)Why can't you turn on the load after efuse fully powers up?
3) can you test after reducing the output cap? this might improve.
thanks,
Hemanth.
Hi Hemanth
1) Yes, without the load, it works as expected.
2) That could be the next step. Wanted explore other options before a PCB change.
3) Yeah I will try that.
Thank you