Part Number: TPS22996
Other Parts Discussed in Thread: TPS22918, TPS2561, TPS22991I, TPS22976
Hi,
I am designing an FPGA board with several power rails. In order to reduce the number of switching regulators, I would like to use load switches to split the rails.
This means that the TPS22996 outputs may drive a high capacitive load and/or an inductive load, if a PI filter is used. Should I be concerned about this?
If this device is not suitable, could you please recommend a load switch for 1.8 V and 3.3 V rails, with 0.5 A output current? An EN pin is mandatory, and a device without VBIAS is preferred.
Thanks.