Hi,
I am bringing up the UCD9224 eval kit, and when I supply +12V for Vin, the on-die Vref is read as only 1.29V (and 0.64V if I supply +5V). This locks me out of testing Vout due to false Vin UVLO failure. I can trick it by setting a really low UVLO trigger, and then Vout operates, but also comes out at a wrong voltage (~2.5V if I set 1V). The calibration routine locks me out of extreme adjustments (as it should). Is there something I need to change on the eval kit HW/SW for Vref to be correct, or do I have a bad part?
Also, for my end design I want to run +5V only, and the silkscreen and part spec say this is ok, but the EVM guide only describes hooking up +12V. Is there any restriction to use 5V (like will the internal ADCs not have full range unless +12V is supplied?). Thanks! Andrew.