This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NI-8451 I2C communication with BQ20z60 - Block Write Issues



I am developing as well as supporting multiple testers for LION battery packs with various different TI chips.  Most have been designed with EV-2300 communications modules but a few have NI-8541's for talking to onboard i2C memory.

I can do everything with the EV-2300 and have no problems.  I have several testers that use the NI-8451 to talk on the SM Bus.  I can read registers and do block reads of the data flash as well as write simple registers, but I can't seem to find the magic incantation in order to do block writes. 

Has anybody done block writes to a TI chip using LabView and a NI-8451?  If someone can get me going, I will write up a set of LabVIEW vi's that encapsulate the whole process much as the EV-2300 dll has.

Tom Houston

970-391-8927

tom@testengineeringconsultants.com