Other Parts Discussed in Thread: BQWIZARD, BQ78PL116, BQ76PL102
I am getting an error message "Error Reading Data" when I use bqWizard 3.1.0 to access bq78PL116 on the PCB board that I designed, which has one bq78PL116 chip only, in contrast to the evaluation module bq78PL116EVM. I have been testing with the evaluation module, now moving onto designing my board whose schematic is almost same as the evaluation module except for having no bq76PL102. (To be accurate, one bq76PL102 is on my board but it is electrically disconnected now for debugging purpose) I am thinking that not having bq76PL102 might be causing this problem. I am wondering if this is the case, or there are any other reasons.
The message window of "Error Reading Data" says "An error has occurred while reading the parameters. The data displayed may not reflect any recent changes. What would you like to do?". Then the reading progress indicator right below the menu bar of bqWizard stops with "Reading Parameters 1%" displayed. Other errors I got are "0 cells found" after initialization, and "LAN is not built. The expected number of cells did not equal the actual number of cells reported by the hardware" after commanding "Connect to Pack (F2)".
I know anyone would be skeptical about my PCB board first. However many functionality works fine. I am able to get parameter values by "Read this parameter" while "Read all Parameters" results in "Error Reading Data". I can rewrite some parameter values successfully. Firmware 6000 built 719, Pack Configuration file(.tmap), and Chemistry data were downloaded without problem, which I confirmed by checking relevant parameters. The voltage at VLDOs are correct. I can switch on and off DFET, CFET, and PFET by writing "Algorithm Enable" parameters. Safe-disconnect works as expected with two LEDs flashing.
There are posts about the problem similar to mine, such as:
http://e2e.ti.com/support/power_management/battery_management/f/180/t/123611.aspx
http://e2e.ti.com/support/power_management/battery_management/f/180/t/88119.aspx
neither of them gave me any useful solution.
Any suggestion is greatly appreciated.
Iai