Hi to all,
I read the spraab3 pdf (http://www.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=spraab3) and using matlab , for a computation delay of 0.5Ts (pag 9 pdf , were Ts= sampling time of 4e-6 sec) i see a 38% overshoot for the step response. I used the model of the plant and the controller that appears in the pdf (pag 9, discrete models) to do the step response.
I want to know if this is correct and i have a few questions about it:
1) This overshoot would damage the electronics connected to this dc-dc converter?(I guess it would... )
2) ways to reduce this overshoot, trying to maintain the controller specifications?
Thanks for your answer, i´m trying to build my own dc-dc converter.
Regards.
Gastón