IThe TPS2540 data sheet specifies Rds(on) as having a maximum value of 120 mohms. I am seeing considerably higher values .38V @ 1.44 Amps, or 260 mohms. The conditions are Vin=5.0 volts, ILIM0= hi Z, ILIM1=24.9K, ILIM_SEL+Vin. The highest case temperature I am measuring is about 80-82C. I am measuring the voltage right at the pins of the device with simultaneous current measurements downstream at the load resistor. I notice the voltage drop across the switch seems to decrease with temp, contrary to figure 8 in the data sheet. A measurement made within the first second or two of the load being applied to a cold board gave me a reading of .43V @ 1.47A, or 292 mohms.
Is the specification incorrect, or am I doing something wrong?