This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq78PL116 BOD circuit active threshold

I heard BOD circuit becomes active when odd cells input voltage is below 2.8V.

But I think that the threshold is 2.7V. Because VLDO didn't shut down when odd cells input is higher than 2.7V though EUV was detected.

When odd cell voltage is below 2.7V, VLDO shut down.

Is my idea wrong?

If my idea is right, I think EUV threshold must be set below 2.7V.