This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Application Note SLVA139

Table 1 on page two show two IRF components: ILRML2502, ILRML6401

However, I could only find IRLML2502 and IRLML6401.

If I read the datasheets right, they show:
the RDs for IRLML2502 as 80 mOhms at 2.5V not 2.7V
and for IRLML6401 as 85 mOhms at -2.5V not 2.7V.

Jon