Hi,
below, you can see a design that I maded to test the BQ2014H gas gauge.According to the application note SLUA40, I realized the software to achieve HDQ communication with BQ2014H but the presence doesn't detect after generate a break to reset the communication and after several attempts, communication is still not working. May be the problem is hardware.
that is my configuration
sense resistor | 0,10 Ohm | |||||||
Number of Cell | 4 | |||||||
capacity | 2100 mAh | |||||||
current range | 50 mA | to | 1 A | |||||
self-dicharge | NAC/47 per day 25 °C | |||||||
voltage drop | 5 mV | 100 mV | ||||||
Nominal discharge | 1,2V | |||||||
PFC | 210 mVh | ------> | PROG5 | L | NAC/47 | |||
PROG4 | L | PFC= 33792 | SCALE= 1/160 | |||||
PROG3 | Z | |||||||
PROG2 | Z | |||||||
PROG1 | Z |
Please, can someone help me ?.
Thanks