This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boost Controllers for 3.3V to 12~24V conversion

Other Parts Discussed in Thread: TPS61170, LM2731

Hello sirs.
I have a PCB where I have a precision 3.3V power supply with 1A capacity.
I will need another power supply with 12V or 15V or 20V or 24V capable of supplying around 80mA DC, generated from this 3V3 rail.

I will change the PCB layout when needed, and the only power source available to generate the "boost" voltage is the 3.3V rail.

Somebody recomends controller ICs for this purpose?

I have many types and values of inductors here so I just need to get some samples of some controller ICs, to test them in practice.

This power supply can be not insulated (no need of a flyback insulated design). 
I can buy the Boost controllers on Digikey.

The parameters are:

3.3V -> 12V (80mA or more, if possible)
3.3V -> 15V (80mA or more, if possible)
3.3V -> 20V (70mA or more, if possible)
3.3V -> 24V (60mA or more, if possible)

Recommendations?

This power supply will be used in supersonic applications. Help?