In my actual design I use a TPS40055 (24V input, 3.1V output 15A). But I need more output current and I read in the datasheet that the TPS40054 allows paralleling of converters.
From the datasheet:
"The TPS40054 operates in one quadrant and sources output current only, allowing for paralleling of converters
and ensures that one converter does not sink current from another converter. This controller also emulates a
non-synchronous buck converter at light loads where the inductor current goes discontinuous. At continuous
output inductor currents the controller operates as a synchronous buck converter to optimize efficiency."
These are the only informations I get until now.
Do I have to change my design or is it possible to operate two my converters?