Hi
I have recently bought a bq78PL114S12 –EVM running FW5000 monitoring 3 18650 cells which have been charge/discharge cycling in the default 3S1P. All of the functions of the BQwizard look to be working except I cannot get FCC to change above 2400mAhr. I have tried different cell chemistries, design capacities and set up 3S2P pack configuration but FCC never goes higher than 2400mAhr. Surely if you specify 2P or design capacity set at 4800mA then one might expect FCC to start at 4800mAhr (following initial setup/relearn). FCC does adjust itself down as expected during chg/disch depending on load etc. (Qmax is also always 2400mAhr.)
Other puzzling issues are: 1) Following a charge when CC is set then SMBdata “Fully charged” is set, but once set it never clears again even when battery discharges to when DC is set. 2) When DC sets and discharge FET is switched off I never get SMBdata “Fully Discharged” go green. 3) When I set up 4S1P pack configuration FCC stayed at 0 and Qmax for cell 4 (only) also was 0. I was recording voltage from cell 4 and parameters have always looked correct ie pack configuration being shown as expected.
All of the above makes me think either I have missed a key point or perhaps the 78PL114 within the EVM is not fully functional. I have read all the application notes/documents. I have been all around the functions of BQ wizard including logging to see what is available. The only thing I have not yet done is set up a (.AUX) file which I don’t think I need yet to just evaluate the system.
So if I have 4 18650E batteries in parallel (2550mAhr x 4) how do I set up wizard to set FCC (initially) to be 10200 mAHr? Running the BQ2060A EVM software one is able to program a "last discharge capcity" figure into the EEPROM. Can you do similar with the 78PL114?
Any help/suggestions gratefully received. Deadline looming!
Thanks, Bob