Hi ALL,
In one of my application I need to generate 3.0V o/p. I found two regulators LM317 (which we used earlier) & TPS71530 (which I want to use). I have several questions regarding this:
1. In datasheet of LM317, o/p cap of 1uF electrolytic is advisable & in TPS71530 its .47uF (or greater) ceramic or tantulum. Do different type of capacitors effects differently in voltage regulators. Like using 1uF electrolytic in TPS71530 produce different results as compared to 1uF ceramic?
2. In LM317, 1uF is preferred at o/p. Do that 1uF is suitable for entire current range of o/p current 0-1.5A, (limit of LM317 )or higher value cap is needed, if current increases.In brigde rectifiers I read that with increase in current cap value also increases. Do the same applys here also.
3. What are the factors by which input & output capacitors values are calculated in an application?
4. I found some application notes, but they consider frequency factor also. Is it noise. But noise in circuit is not having some constant frequency.
Aamir Ali, TE
DAS