This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Choosing a microcontroller for fuel cell application

Hi,

I am designing DC DC converter of high voltage boost using an isolated topology( transformer) for fuel cell applications.The input DC voltage is 50 V and the output voltage is 300 V.The DC is inverted to 3 phase AC using H bridge and then using a high frequency transformer,its boosted to 300 V(Vrms) and then its rectified to get an average DC output votlage of 300V.I had chosen International rectifier IR 2184 as the gate driver IC  for switching the high frequency MOSFET's .For my current applications,I wanted use  the controller which would be more compatible.looking forward for valuable suggestions.