Hi All,
I am having some trouble with BI/TOUT activity disturbing some sensitive analog parts near BQ27510, and I would like to know if did any of you have the same issue. It seems that BI/TOUT actually pulls-up (data sheet states that the pin is pulled LOW) every second the NTC network to check if there is a battery connected. But there is a 33nF capacitor connected at the BI/TOUT pin to GND, that cause a current inrush when the BI/TOUT is pulled up, since, with the battery connected, the termistor will put the network voltage value near zero. Is that correct? If yes, can I put a resistor at BI/TOUT pin to damp the current inrush into the capacitor? Will this resistor affect my battery temperature measurement? what is the maximum resistor value could be used in this case?
Thank you,
Renato