I have a circuit (see attached) provided by an LCD manufacturer that illustrates using the POL signal from the display to derive the VCOM signal. From what i've read, LCD Bias ICs generate VCOM from the high bias voltage. Is it possible to instead feed the POL signal into one of these ICs to generate the VCOM signal? Is there a version of these ICs that provides a 'discrete' opamp that can be utilized as illustrated in the attached schematic?
For reference, VR50 adjusts the gain of VCOM which affects the color saturation. VR51 provides contrast adjustment by level shifting the VCOM signal.
Thanks!