This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Disabling VBUS Wake-up on TPS65950

Hello,

On our prototype, we make the USB-OTG port available to a docking station via a set of gold contacts molded into the bottom of the device.  We discovered that sometimes the device could be turned on when these contacts were touched.  I did a little more research, and found that any time there's a voltage on VBUS over 550mV, this sends a signal to the power manager module to power on the device.  I read through the relevant sections of the TRM, and tried making adjustments to the kernel to ignore this interrupt, but to no avail.  I tried the following things:

-Set USB_PRES_RISING within PWR_EDR1 to 0.

-Set USB_PRES within PWR_IMR2 to 1.

-Set USB_PRES within PWR_IMR1 to 1.

-Set USB_PRES within PWR_ISR1 to 1.

All of these steps were done individually, and all with the goal of having the power module ignore the interrupt generated by the VBUS Wake-Up interrupt.  What's wrong with my method or can this even be done?

Thanks,

Jake