There is a question about the soft start of TPS65150.
(Please look at the 13th page of the data sheet. )
1.Is the clock cycles equal to switching frequency?
2.Does the start-up time of input voltage have restriction?
・Is it required 5ms or more?
・Do any problems occur at the time of less than 5ms?
3.Is the input voltage power supply of the characteristic data of data sheet figure 8 supplied?
I would appreciate your favor which will be saved if you can advise .