Hi,
I am using LM5021 to do a AD-DC voltage
converter, with an output of 5 Volts. My circuit in the beginning has 5.025
Volts in the output, but after 2 seconds (more and less) he starts oscillating,
like 2.4 Volts, then 4.5Volts and 5.025V, and he keeps like that all the time.
I am using a 65 ohm resistance, which means about 70mA. The problem must be the
transformer? In Cs pin, or comp?
Regards,
Rui Duarte