Hi all,
I'm designing a charging circuit based on bq24032A and I want to pull ISET2, PSEL & CE HIGH, and for the sake of simplicity I plan to pull the three of them up with a unique resistor.
Reading the datasheet I see that there are some input current limits in the electrical characteristics for these inputs, which for the max value read: 40uA for ISET2, nothing for PSEL and 1uA for CE. Are these values about the max current those inputs will draw? or is it the max current that can be input into them?
My Vcc is from USB or AC through some schotty diodes, so the voltage would be around 4.3-5v, and I'm using right now a unique 100k resistor for the pull-up for three of them. Does it look ok to you?
Thanks,
Asier.