Hi,
We are use TPS54425 to convert 12V input to 5.1V output. 3-4A max.
Schema is equal to TPS54425 data sheet, except: R1=22K1, R2=3k9, L1=3,3uH.
In data sheet, OCP (Overcurrent protection) and protections UVLO, UV, LO are no latching.
"EN" is permanently connected to Vin (12V).
Problem:
- if a short circuit and over current Vout is disconnected permanently until deactivated and active again
- if there is a 2200uF capacitor in parallel with Vin or Vin rises slowly with EN permanently connected to Vin, Vout = 0V. No output voltage
Regards,
Jose Garcia.