Hi,
I designed a DC-DC solution using the LMR62421, and just got the PCBs back from the producer. However, seems like I've made a mistake and forgot to include the feedback capacitor which is supposed to connect Vout with the feedback pin on the DC-DC IC. What are the consequences of this? Might it still work? I haven't assembled the components on the PCB yet, wondering if I should do that, or simply get a new PCB produced.
Thanks!