In accordance with the datasheet of the bq33100 the resolution of the calculated capacitance is in Farad. Are there any possibilities to increase this resolution of the capacitance mesurement of the bq33100?
For example, if I use a stack of 5 capacitors with each 25F @ 2,1V, I get a total capacitance of 25F/5=5F. In this example the resolution of 1F (20% of initial value) is insufficient.